Advanced Settings
How do I open Advanced Settings?
- From theStartmenu, selectRockwell Software>FactoryTalk Linx Gateway Configuration.
- ExpandOPC UA Server, and then selectAdvanced Settings.
The following table shows the settings on
Advanced Settings
. Field | Description |
|---|---|
Maximum anonymous client connections | Configures the maximum anonymous connections. FactoryTalk Linx Gateway
supports up to 100 connections, the total number of anonymous and secured
connections. The default is 50 connections. If the configuration was restored from
a previous version, the field will be set to 100.For more information, see Maximum anonymous connections. |
Create additional references for each array element in the OPC UA namespace | When selected, FactoryTalk Linx Gateway will support OPC UA clients to browse sub-elements under array.Tip: This option is only available when Tag list and structure/array access on OPC UA Server is selected. |
Cache OPC UA Server namespace | Select this checkbox to create a cache for UA Tag List and Custom UA Namespace. Cache UA Server namespace checkbox is cleared by default. Changing the UA Tag List and Custom UA Namespace configuration will recreate a cache. For more information, see Cache OPC UA Server namespace. |
Refresh | It is available when the Cache UA Server namespace checkbox is selected.Note: Based on the number of tags defined in the namespace, this could take an extended period of time to complete. |
Enable configuration of OPC UA namespace index | Selects this checkbox to specify, refresh, delete, import or export OPC UA namespace index when tag list is turned on. For more information, see Enable configuration of OPC UA namespace index. |
Namespace index presented to OPC UA clients | Sets user option to select FactoryTalk Linx Gateway
OPC UA service namespace index value. An OPC UA Client will see (2 or 3). Default is 2.
|
Namespace URI | Changes the namespace URI text string for the namespace index that you select to
present to the OPC UA client. It is only supported for Folders with scalar data
and Tag List. |
Provide Feedback