Enable configuration of OPC UA namespace index
A "namespace index" is a number a client can utilize to identity the data to be accessed from an OPC UA server. Changes to the configuration may cause the namespace index values to also be modified, causing difficulty for some OPC UA clients. FactoryTalk Linx Gateway provides the ability to override the default namespace index numbers and assign numbers to help OPC UA clients connect to the service.
With the
Enable configuration of
option turned off:OPC
UA namespace index- A single namespace index is used for data fromFactoryTalk Directory.FactoryTalk Linx Gatewaypulls data from multiple tags and structures which can exist in multiple controllers that use the same datatype name with the prefix [Shortcut name] but defined by a different layout.
With the
Enable configuration of
option turned on:OPC
UA namespace index- The namespace index can represent each data source ofFactoryTalk Linxshortcuts or UA Connector endpoints to avoid a collision where two sources have different types with identical type and tag names. The common index is 10 for other types of data servers.
OPC
UA namespace index valueThe valid range of namespace index is from 0 through 9999.
By default, a new index is assigned for a new added
FactoryTalk Linx
shortcut or a new added UA Connector endpoint.To edit the index
- Select the tag row and then click
.TIP:- If a tag ID starts with ''[xxx]'' fromOPCDA Data Server (for example, tags that originate from RSLinx Classic), it will have an individualOPCUA namespace index not the common index as 10.
- We don’t recommend an index sequence with large gaps.
Provide Feedback