Maximum anonymous connections

Clients can connect to the OPC UA interface as anonymous or secured with a username and password. FactoryTalk Linx Gateway supports up to 100 maximum connections. This option permits the user to limit the total number of anonymous connections to ensure that secured connections are available. The default setting is 50 anonymous connections.
  • Total of 100 anonymous and secured connections
  • Connections used on a first come basis
  • Anonymous connections limited by this setting
  • Secured connections limited by the number of available connections
With Maximum anonymous connections = 50
Anonymous connections used
Secured connections available
No anonymous connections
0
100
Some anonymous connections
25
75
Maximum anonymous connections
50
50
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal