Namespace mode
FactoryTalk Linx Gateway provides these namespace modes.
Field | Description |
|---|---|
Folders with scalar data |
|
Tag list and structures/array access |
|
Custom namespace |
|
The following table shows the supported namespace modes of each server using the
FactoryTalk
application and standalone data service. Data source | Interface | Folder with scalar data | Tag list and structures/array access | Custom namespace |
|---|---|---|---|---|
FactoryTalk Application | OPC UA Server | Yes | Yes | Yes |
MQTT | No | No | Yes | |
OPC DA Server | Yes | No | No | |
RTD Server | Yes | No | Yes | |
DDE Server | Yes | No | Yes | |
Standalone Data Service | OPC UA Server | No | No | Yes |
MQTT | No | No | Yes | |
OPC DA Server | Yes | No | No | |
RTD Server | Yes | No | Yes | |
DDE Server | Yes | No | Yes |
Provide Feedback