- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
User-defined data types
A data type specifies the size and layout of memory that allocates when a tag of the data type is created. The core of the control system is defining operations based on data stored in tags. Tags support different types of data that define the size and layout of memory that is allocated for the tag.
Data types can be atomic, structure, or array and categorizes as predefined, module-defined, and user-defined.
Provide Feedback