Device definition

Device definition

Use these elements to define a device. These elements are common to all device definitions.
deviceCategory
defines the type of device.
Element
Description
ControllerDevice
Defines this instance as a controller.
CipDevice
Defines this instance as an active device, such as an adapter, an IO device, and so on.
See Device definition for an example of device definition syntax. See Controller example for an example of controller definition syntax.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal