- Using the software
- Ladder Editor
- Add-On Instructions
- Instructions
- Instruction set
- Code Editor Domain Specific Language Syntax
Create a project
Create a project to build your system design. All projects are stored in a remote repository to provide access to collaborators. When changes are pushed to the remote repository, projects with controllers generate L5X files that are stored within its FactoryTalk Vault Solution.
Project names must adhere to the following rules:
- The first character must be a letter.
- The subsequent characters can be letters, numbers, or underscores.
- The last character must be a letter or a number.
- The project name must be at least two characters, with a maximum length of 40 characters.
- The project name cannot end in the reserved phrasel5xconvert.
Create a project from the
Welcome
page or the File
menu.
TIP:
You can have only one project open at a time.
- Close any open project.
- Either:
- On theWelcomepage, selectNew project.
- From the menu bar, selectFile > New project.TIP: The first time you open a project in FactoryTalk Design Studio, theGetting Startedpage opens with information about features to start using FactoryTalk Design Studio. To close theGetting Startedpage, in theGetting Startedtab, select
. To reopen the
Getting Startedpage at any time, in the main toolbar, selectGetting Startedfrom theHelpmenu.
- InNew project, inName, enter a unique name for the project.
- InProject Location in the FactoryTalk Vault, choose from an existing list of solutions or create and name a solution.TIP: To share an existing project, with the open project, selectFile > Source control > Share project.
- SelectCreate. FactoryTalk Design Studio creates the empty project.
Provide Feedback