Material phase binding
Material phase binding is the process of either:
- Binding unbound material-enabled phase steps to a material phase and associated container
- Rebinding a previously bound material-enabled phase step within a control recipe
When configuring an operation recipe's step that references a material phase class, the operator can select one of the three types of binding:
- A specific material phase and container. The operator chooses a specific phase and container pair from the list.
- Automatic: TheFactoryTalk BatchServer selects the equipment phase associated to the highest-priority container.
- Prompt. The operator must select a phase/container while the recipe is running.
To perform material binding, these criteria must be true:
- The step is associated with a material-enabled phase class in the recipe.
- The step is inactive or has a status of BINDING.
Provide Feedback