Respond to a material phase binding prompt
Material phase binding prompts are displayed when the operator has set up prompted binding for material phase/container pairs. Respond to the binding prompts to select a material phase/container pair when the recipe is running.
To respond to a material phase binding prompt
- SelectBatches.
- Select a batch.
- In theBatch Detaildisplay, selectStartto execute the recipe.The recipe is running, and a prompt alert is displayed.
- Navigate to thePromptslist and select the material phase binding prompt for the recipe that is running.
- Select a material phase/container pair from the list.
- SelectAcknowledge
.
Provide Feedback