Manually bind a phase instance and associated container to a material phase step

A configured material requirement of the operation recipe’s step gives the
FactoryTalk Batch
Server and Material Server enough information to select and bind a phase instance and its associated material containers to a batch. As a result, the correct phase that has access to the ingredient required is selected and run.
Manually binding a material-enabled phase step requires the operator to select not just a phase, but the container the phase is associated with, and depending on the material container type, the exact sublot (a specific measured amount of an ingredient) to be used.
In an operation control recipe, an operator can manually bind a phase instance and associated container to a material phase that is referenced by an operation step. A previously bound material phase step can also be manually unbound and rebound to a different phase/container. You can also reassign a material phase step for either
Prompt
binding or
Automatic
binding.
A material phase step previously assigned to a phase/container can be reassigned manually to a different phase/container, as long as the material phase step has not already executed.
Prerequisites
To perform manual binding to a material phase step in a batch procedure control recipe, make sure these conditions are met:
  • The selected phase step is material-enabled.
  • If the step is set to
    Prompt
    binding and the
    FactoryTalk Batch
    Server has issued the operator bind prompt, the step is inactive or has a binding status of BINDING on the transition prior to the step.
To manually bind a phase instance and associated container to a material phase step
  1. Open
    FactoryTalk Batch View
    and select
    Batches
    .
  2. Select a batch that has the step that requires binding.
  3. In an operation's
    Batch Detail
    display, select the material phase step.
  4. Select
    Bind
    ftb_vw_bind.
  5. In
    Binding a Material Phase Step
    , select a phase/container pair to bind to the material phase step.
  6. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal