Running material-based recipes
Running a material-based control recipe offers more flexibility in the binding process and the capability to track inventory. The
FactoryTalk Batch
Server and FactoryTalk Batch
Material Server work together to pull the necessary information from the material database so either FactoryTalk Batch
or the operator can select the appropriate containers to supply materials to the recipe.In this chapter, you run a material-based recipe using the
FactoryTalk Batch
Phase Simulator. The Phase Simulator supplies the ACTUAL_AMOUNT and FEED_COMPLETE parameters to enable the batch to run. This data normally is supplied by the phase logic in the process-connected deviceĀ (PCD).Provide Feedback