Running a material-based recipe

  1. Select
    Start > Rockwell Software > View
    .
  2. IMPORTANT:
    Administrator privileges are required to perform this procedure.
    Click the
    Add Batch
    button, select
    MCLS_CHOCOLATE_HAZELNUT
    , and then click
    OK
    . The
    Batch Creation
    dialog box opens.
    FTBMM_GRG_batch_creation
    The deferred the formula parameters display in the
    Batch Creation
    dialog box with the default settings. You can change the values if you need to adjust the recipe.
    In the Unit Binding area, the two alias names you defined are displayed. You can select which units to bind to the recipe. Because there is enough material in all the containers you are presented with both units.
  3. In Unit Binding area, select
    NP_MIXER1
    and
    NP_FREEZER1
    if not already selected.
  4. In the
    Batch ID
    box, type
    BATCH101
    , and then click the
    Create
    button.
  5. Select the batch, click the
    Start Batch
    button, and then click
    Yes
    to start the batch.
  6. Click the
    Procedure as SFC
    button. Adjust the panes, if necessary so you can see the Container column to watch as the FactoryTalk Batch Server binds to containers.
    FTBMM_GRG_columns_B12
  7. When the recipe reaches MBR_ADD:2 under MCLS_CHOCOLATE_HAZELNUT_OP:1 notice that the batch binds to NUT_BIN3 and the priority of 10 shows in the Index column. After the phase is complete, the Container setting changes to NULL_CONTAINER.
  8. Let the batch run to completion.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal