Configuring materials
The Material Editor is used to facilitate easy configuration and manipulation of the material-based recipes database. Material configuration is the process of adding, editing and deleting various material data that is stored in the material database.
Provide Feedback