Deleting materials
- In either the Hierarchy pane or Detail pane, right-click the material to delete, and then click theDeletebutton.
- If theConfirm deletionuser preference is enabled, you are asked to verify the deletion. To delete the material, clickYes; to cancel the deletion, clickNo.If theConfirm deletionuser preference is disabled, the selection is deleted without a confirmation message. (See Configuring the Material Editor for more information.)
Provide Feedback