Configuring the Material Editor
There are several settings you can choose from to configure the Material Editor. You can turn on information tips, change the text and background colors of the application, configure the various views, and set up reports used for printing recipe data. You can also change the location of the Material Server.
Provide Feedback