Configuring material lots

The
Lots
tab contains the information that identifies a particular quantity of a material. A lot holds all of the static information about the lot, such as Lot Identifier, Material Type, State of the lot, Engineering Units, and Controller ID value. A lot may also contain sublots, which detail the actual quantity of the lot that is distributed into material storage containers. An example of a lot could be: Shipment number SN2009 of the material Granulated Sugar, which is part of the material class Sweetener and is classified as a
Raw
material type.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal