Editing a lot

You can change the material’s properties and the amount of material in the lot, and distribute a lot of material to a container.
  1. From the
    Edit Material
    dialog box, select a record row to edit, and then click the
    Edit Lot
    button. The
    Edit Lot
    dialog box opens to the
    General
    tab.
    FTBMM_ED_odin_edit_lot_general
  2. Modify the general lot information as needed, and then click
    Apply
    .
  3. Select the
    Properties
    tab. The properties assigned to the lot of material display. You can change the value of the property directly in the
    Value
    column or use a form.
    FTBMM_ED_odin_edit_lot_properties
  4. In the
    Value
    box, type a new value for the property.
    IMPORTANT:
    If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
  5. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal