Using a form to change lot properties

  1. On the
    Properties
    tab, select the record row to edit, and then click the
    Edit Property
    button. The
    Edit Lot Property
    dialog box opens.
    FTBMM_ED_Edit Lot Property
  2. In the
    Value
    box, type the value of the property, and then click
    OK
    .
    IMPORTANT:
    If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal