Changing a sublot quantity

  1. TIP: If you edit a sublot by distributing the lots of material, deleting a distribution, or changing the amountn of material, the material's inventory information also changes.
    From the
    Edit Lot
    dialog box, select the
    Storage
    tab. The distributed amounts of the lot display.
  2. Select the record row to edit, then click
    Edit Distribution
    .
  3. IMPORTANT: If you are changing a value that contains a decimal, use the
    Delete
    key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
    Type a new amount in the
    Quantity
    box.
  4. Click
    OK
    to return to the
    Storage
    tabon the
    Edit Lot
    dialog box.
  5. Click
    Apply
    to save the changes, or click
    OK
    to save the record and close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal