Configure material inventory
The for more information).
Inventory
tab displays a view of the material lot distribution. Each row represents a sublot. A sublot is an amount of material in the selected lot that is distributed to a container. The container, lot, and label are used by the FactoryTalk Batch
Server when searching for a material to bind to a recipe. When the recipe is complete, the FactoryTalk
Batch Server updates the amount to reflect the amount of material either consumed from the container (Addition) or added to the container (Distribution). You configure the container type in the FactoryTalk Batch
Equipment Editor. (See the FactoryTalk Batch
Equipment Editor User ManualWhen you edit, distribute, or delete a distribution in a material’s inventory, the results also affect the container’s inventory.
Provide Feedback