View alarm faults (Banner)

Use the
Alarm Faults
dialog box to view the alarm fault list. An alarm fault occurs when there is a problem with an alarm condition. This could be a configuration error, a problem getting the value of an Input Tag or Limit tag, or a problem communicating with a device producing an alarm.
To view alarm faults
  1. On the status bar of the Alarms and Events Banner, either:
    • Double-click the
      Alarm Faults
      panel FTAeStatusPanelAlarmFaults
      or
    • Right-click an alarm and then click
      View Alarm Faults
      .
  2. Click
    the close (
    X
    )
    button
    to close the
    Alarm Faults
    dialog box.
    TIP:
    The
    Alarm Faults
    dialog box does not display faulted alarms that are disabled or suppressed. It only displays the most recent 500 alarm faults.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal