Alarm and Event Banner Properties - Event Subscriptions tab

How do I open the Alarm and Event Banner Properties dialog box?
Properties are modified during design time. To open the
Alarm and Event Banner Properties
dialog box:
  1. Open FactoryTalk View Studio.
  2. Add an Alarm and Event Banner object to a display.
  3. Right-click the Alarm and Event Banner object, and then click
    Properties
    .
To subscribe to events that match specific criteria use the
Event Subscriptions
tab in the
Alarm and Event Banner Properties
dialog box.
The
Event Subscription
tab contains a default subscription which includes all areas, priorities, and event sources. When a new subscription is created the default subscription is removed. You can specify as many, or as few, criteria as you need when creating an event subscription.
Multiple subscriptions are combined together. The subscription criteria are combined using the logical AND operator. For example, checking only the priority Urgent, entering an area of
Packaging Line
and entering an event source of
[BoxStuffer]*
will subscribe to Urgent alarms from the packaging line whose names begin with [BoxStuffer].
The following table provides details about the settings on the
Event Subscriptions
tab and how they can be used:
Setting
Description
Event subscription list
Displays the subscriptions currently configured for the Alarm and Event Banner.
Add
Used to add a new subscription.
Subscription name
The name given to the subscription when it was created.
Rename
Used to provide a new name for an existing subscription. All event subscription names must be unique.
Remove
Used to remove the subscription and stop filtering alarm events on the subscription criteria.
Priority level
Identifies the priority level of events displayed in the Alarm and Event Banner.
Urgent, High, Medium, Low, Event
Used to filter alarm event based on priority level.
Scopes list
Identifies the scope used to determine the events forwarded to the Alarm and Event Banner.
The default scope is
(Any Scope)
, which is equivalent to selecting the top node in the
Select Scope
browser.
Browse
Used to subscribe to events that fall within a given scope.
Event sources list
Used to select specific areas, servers, or groups from which to monitor alarms using the Alarm and Event Banner.
Browse
Used to identify specific alarms to subscribe to by browsing a list.
Add
Used to identify specific alarms to subscribe to by providing the alarm name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal