Use the Alarm and Event Banner at runtime
At runtime, use the Alarm and Event Banner to interact with alarms and events and view alarm faults.
If your HMI display does not have a mouse or a touch screen, use the following keyboard short cuts to navigate the display:
Use this key | To do this |
---|---|
HOME | Select the first item in the alarm list. |
END | Select the last item in the alarm list. |
UP Arrow | Select the previous alarm in the alarm list. |
DOWN Arrow | Select the next alarm in the alarm list. |
ENTER | Execute the double-click action on the selected row. |
Provide Feedback