Recreate a deleted user account
All user accounts are identified using a unique identifier that is separate from the user name. Deleting a user account also deletes the user's access rights but does not delete the user account's unique identifier. When creating a user account with the identical name, the new user account does not automatically have access to the same resources as the previous account.
When creating another user account with the same name, recreate the security settings of the account. Either add the user account to a group with defined security settings or create permissions for a user account when securing a resource.
The account must have the security policy
Keep record of deleted accounts
set to disabled
to create an account using the name of a previously deleted account.Prerequisites
Obtain these permissions in the
Users
folder in FactoryTalk Administration Console
Explorer
:- Common > Create Children
- Common > List Children
- Common > Read
To recreate a deleted user account
- Add a new user account. Choose one:
- If the security policyKeep Record of deleted accountsis disabled, create an account using the same name as deleted account.
- Recreate the security settings of the deleted account on the new account. Do one:
- Add the user account to a group with the proper security settings defined
- Set permissions for a user account when securing a resource
To delete a user account from both
FactoryTalk
directories, delete the account from one directory and log off that directory. Log on to the second directory and delete the account in the second directory.Provide Feedback