Enable a user account
When a
FactoryTalk
user account is disabled, the account is present, but cannot be used to log on to the system. A FactoryTalk
administrator can manually enable an account.A
Windows
-linked user account cannot be enabled in FactoryTalk Administration Console
. Use Windows
to enable a Windows
-linked user account.Prerequisites
Enabling a disabled user account requires these permissions:
- Common > List Children
- Common > Read
- Common > Write
To enable a user account
- InFactoryTalk Administration ConsoleExplorer, expandSystem>Users, right-click the user account and selectProperties.
- InUser Properties, clearAccount is disabled,and selectOK.You can also use Historical Usage to enable a user account.
User accounts in the network directory are separate from accounts in the
FactoryTalk
local directory. To enable accounts in both directories, enable the account in one directory, log off that directory, log on to the second directory, and enable the account in the second directory.Provide Feedback