HSC instructions
Use high-speed counter (HSC) instructions to monitor and control the high-speed counter.
Instruction | Description |
|---|---|
HSC applies high presets, low presets, and output source values to the high-speed counter. | |
HSC_SET_STS manually sets or resets the HSC counting status. | |
HSCE starts, stops, and reads accumulator value. | |
HSCE_CFG is the high-speed counter configuration. | |
HSCE_CFG_PLS is the high-speed counter Programmable Limit Switch configuration. | |
HSCE_READ_STS reads high-speed counter status. | |
HSCE_SET_STS manually sets/resets high-speed counter status. |
Provide Feedback