HSC_SET_STS (high-speed counter set status)
HSC_SET_STS manually sets or resets the HSC counting status.
Operation details: The HSC function block must be stopped (not counting) for the HSC_SET_STC function block to set or reset the HTS status. If the HSC function is not stopped, the input parameters continue to update and changes made using HSC_SET_STS are ignored.
Languages supported: Function block diagram, ladder diagram, structured text.
This instructions applies to the L50E and L70E controllers.
HSC_SET_STS

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | Instruction block enable.
|
HscID | Input | UINT | Manually sets ore resets the HSC status. |
Mode1Done | Input | BOOL | Mode 1A or 1B counting is done. This bit can be set or reset when HSC is not counting. |
HPReached | Input | BOOL | High preset reached. This bit can be set or reset when HSC is not counting. |
LPReached | Input | BOOL | Low preset reached. This bit can be set or reset when HSC is not counting. |
OFOccurred | Input | BOOL | Overflow occurred. This bit can be set or reset when HSC is not counting. |
UFOccurred | Input | BOOL | Underflow occurred. This bit can be set or reset when HSC is not counting. |
Sts | Output | UINT | Status codes are defined in HSC status codes (Sts). |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. |
HSC status codes (Sts)
Status Code | Status Description |
|---|---|
0x00 | No action taken (not enabled). |
0x01 | HSC execution successful. |
0x02 | HSC command invalid. |
0x03 | HSC ID out of range. |
0x04 | HSC configuration error. |
HSC_SET_STS examples
HSC_SET_STS function block diagram example

HSC_SET_STS ladder diagram example

HSC_SET_STS structured text example

Provide Feedback