HSCE_SET_STS
The instruction manually sets and resets the HSC counting status flags. The HSC function block must be stopped for the HSCE_SET_STC function block to set or reset its HTS status. If the HSC function block is not stopped or the HSC channel is not configured, the HSC2_SET_STS function block will throw an error.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L20E, L50E, and L70E controllers.
HSCE_SET_STS

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | Function block enable.
|
Channel | Input | HSCE_CHANNEL | The HSCE channel. |
HPReached | Input | BOOL | When the high preset value is reached, this bit will be set to TRUE by the plug-in module. Set or reset this bit by the HSCE_SET_STS function block. |
LPReached | Input | BOOL | When the low preset value is reached, this bit will be set to TRUE by the plug-in module. Set or reset this bit by the HSCE_SET_STS function block. |
OFOccurred | Input | BOOL | When overflow occurred, this bit will be set to TRUE by the plug-in module. Set or reset this bit by the HSCE_SET_STS function block. |
UFOccurred | Input | BOOL | When underflow occurred, this bit will be set to TRUE by the plug-in module. Set or reset this bit by the HSCE_SET_STS function block. |
TouchProbe | Input | BOOL | When the touch probe is triggered, this bit will be set to TRUE by the plug-in module. |
Hold | Input | BOOL | When HSC hold is triggered, this bit will be set to TRUE by the plug-in module. Set or reset this bit by the HSCE_SET_STS function block. This input parameter is only effective for counter 0. Counter 1 is always reset |
Preset | Input | BOOL | When Z ACC Reset is triggered, this bit will be set to TRUE by the plug-in module. Set or reset this bit by the HSCE_SET_STS function block. This input parameter is only effective for counter 0. Counter 1 is always reset. |
Done | Output | BOOL | HSC configuration action (initiated by this instruction) succeeds. |
Error | Output | BOOL | Indicates that an error occurred. |
HSCE_SET_STS examples
HSCE_SET_STS function block diagram example

HSCE_SET_STS ladder diagram example

HSCE_SET_STS text structure example

Provide Feedback