HSCE error codes
The following table describes the status error codes for HSCE instructions.
Error Code | Error Description | Corrective Action |
|---|---|---|
0 | The instruction successfully completed operation. | N/A |
1 | Invalid HSC configuration files. | Contact the Rockwell Automation technical support representative. For contact information, see: |
2 | Invalid HSC module type. | Correct the module type. For example, select the module type as plug-in. |
3 | Invalid HSC Slot ID. | Correct the Slot ID in the Channel input of the function block. |
4 | Invalid HSC ID. | Correct the HSC ID. For example, set 0 for counter 0. |
5 | Invalid mode for the Channel. | Contact Rockwell Automation technical support representative. |
6 | Invalid PLS Size. | PLS size must be <= 24 and the size of the PLS data array must be >= PLS size. |
7 | Invalid PLS offset. | PLS offset + PLS size must be within the size of the PLS data array. |
8 | Invalid InitAccumulator value. | Correct the InitAccumulator value. Maybe it is over the boundary or out range of the LP or HP limit (LP <= InitACC <= HP). |
9 | Invalid LP. | Correct the LP value. It might be over the boundary. |
10 | Invalid OF. | Correct the OF value. |
11 | Invalid UF. | Correct the UF value. |
12 | Invalid HP. | Correct the HP value. |
13 | There is no configuration for HSCE. | Contact the Rockwell Automation technical support representative. |
14 | Invalid HSCE state. | Check the HSCE-related function block to confirm the state of this function block. |
15 | Invalid plug-in module | Check the plug-in module to confirm it is an HSC module. |
16 | HSCE is running. | When HSC is counting, no configuration or setting status is allowed. HSCE_CFG and HSCE_CFG_PLS are executed while HSCE is running. |
17 | Stop HSC plug-in failure. | Contact the Rockwell Automation technical support representative. |
18 | Update rate write failure. | Contact the Rockwell Automation technical support representative. |
19 | Write number of plus failure. | Contact the Rockwell Automation technical support representative. |
20 | Write Apply ACC failure. | Contact the Rockwell Automation technical support representative. |
21 | Write ACC failure. | Contact the Rockwell Automation technical support representative. |
22 | Write Apply failure. | Contact the Rockwell Automation technical support representative. |
23 | Write number of PLS failure. | Contact the Rockwell Automation technical support representative. |
24 | Write under flow failure. | Contact the Rockwell Automation technical support representative. |
25 | Write over flow failure. | Contact the Rockwell Automation technical support representative. |
26 | Write low preset failure. | Contact the Rockwell Automation technical support representative. |
27 | Write high preset failure. | Contact the Rockwell Automation technical support representative. |
28 | Write low preset out failure. | Contact the Rockwell Automation technical support representative. |
29 | Write high preset out failure. | Contact the Rockwell Automation technical support representative. |
30 | Write out mask failure. | Contact the Rockwell Automation technical support representative. |
31 | Write PLS low preset out failure. | Contact the Rockwell Automation technical support representative. |
32 | Write PLS high preset out failure. | Contact the Rockwell Automation technical support representative. |
33 | Write PLS low preset failure. | Contact the Rockwell Automation technical support representative. |
34 | Write PLS high preset out failure. | Contact the Rockwell Automation technical support representative. |
35 | Write PLS offset failure. | Contact the Rockwell Automation technical support representative. |
36 | Write PLS number failure. | Contact the Rockwell Automation technical support representative. |
37 | Read status failure. | Contact the Rockwell Automation technical support representative. |
38 | Read high preset failure. | Contact the Rockwell Automation technical support representative. |
39 | Read low preset failure. | Contact the Rockwell Automation technical support representative. |
40 | Read ACC failure. | Contact the Rockwell Automation technical support representative. |
41 | Read number of pulse width failure. | Contact the Rockwell Automation technical support representative. |
42 | Read pulse width failure. | Contact the Rockwell Automation technical support representative. |
43 | Read number of pulse failure. | Contact the Rockwell Automation technical support representative. |
44 | Read update rate failure. | Contact the Rockwell Automation technical support representative. |
45 | Write status failure. | Contact the Rockwell Automation technical support representative. |
46 | Read low preset out failure. | Contact the Rockwell Automation technical support representative. |
47 | Read high preset out failure. | Contact the Rockwell Automation technical support representative. |
48 | Read PLS number failure. | Contact the Rockwell Automation technical support representative. |
49 | N/A | Contact the Rockwell Automation technical support representative. |
50 | Write apply status failure. | Contact the Rockwell Automation technical support representative. |
51 | Invalid channel input. | Contact the Rockwell Automation technical support representative. |
52 | Read touch probe failure. | Contact the Rockwell Automation technical support representative. |
53 | Write reset ACC failure. | Contact the Rockwell Automation technical support representative. |
54 | Start HSC failure. | Contact the Rockwell Automation technical support representative. |
55 | Counter is disabled. | The HSC counter is disabled. Check the Channel configuration to verify if the HSC counter is enabled. |
56 | Invalid output mask value. | Check if the output mask is within the valid range. For plug-in HSC module, the range is 0–65535. |
57 | Invalid high preset output. | Check the if the HP output is within the valid range. For plug-in HSC module, the range is 0–65535. |
58 | Invalid low preset output. | Check if the LP output is within the valid range. For plug-in HSC module, the range is 0–65535. |
59 | Not a supported UPM revision. | Check the revision configuration for the HSC plug-in module. |
60 | Not an HSC module is added. | Check if the actual plug-in module is an HSC module. |
61 | HSCE plug-in module is not configured. | Contact the Rockwell Automation technical support representative. |
62 | A UPM plug-in Write error occurs while changing HSC plug-in Mode to Non-run. | Contact the Rockwell Automation technical support representative. |
63 | A UPM plug-in Write error occurs while changing HSC plug-in Mode to run mode. | Contact the Rockwell Automation technical support representative. |
64 | A UPM plug-in Read error occurs while reading Output Status. | Contact the Rockwell Automation technical support representative. |
Provide Feedback