Serial Port - CIP serial configuration page
Use the CIP serial configuration page to do the following actions:
- Configure the CIP serial settings.
- Open the communication diagnostics view by selecting theDiagnosebutton.
Setting | Description |
|---|---|
Common Settings | |
Diagnose | Opens the communication diagnostics view, which shows the communication driver status. Diagnose is available when the controller is online and CIP serial or Modbus RTU is set as the driver. |
Baud rate | Lists the baud rate in bits per second. Options are:
The default value is 38400 . |
Parity | Lists the parity bit usage in the communication packets. Options are:
|
Station address | Specifies the station address for the serial port that is associated with the DF1 protocol. The value is from 0 through 254. The default value is 1 . |
Protocol Control | |
DF1 mode | Lists the supported protocol. The protocol control setting varies with the selected DF1 mode. Options are as follows: |
Provide Feedback