DF1 half-duplex master configuration
Use information in the following table to configure a DF1 half-duplex master.
Setting | Description |
|---|---|
Media | Specifies the supported media type. The available options are RS232 and RS485 . RS232 is the default option. |
Control line | Specifies the type of handshake that is used for communication.
|
Error detection | Specifies the error detection scheme for message transmission.
CRC is the default option. |
Polling mode | Specifies the polling mode.
|
Duplicate packet detection | Determines how duplicate messages are handled.
Duplicate packet detection is selected by default. |
ACK timeout | Specifies the duration that the controller waits for an acknowledgment after transmitting a message. The value is from 0 through 32767, with each unit increment representing 20 milliseconds. The default value is 50 (50 * 20 milliseconds, 1,000 milliseconds, or 1 second). |
Reply message timeout | Specifies the channel timeout. If the channel sends a message and does not receive a response within the specified timeout period, the channel will attempt to establish communications again. The value is from 0 through 65535. The default value is 5. |
Message retries | Specifies the count of retry attempts by an slave to retransmit a message packet without an acknowledgment (ACK) from the primary device. The parameter can be used in noisy environments, where message packets might become corrupted during transmission. The value is from 0 through 127. The default value is 3. |
Pre-transmission delay | Specifies the amount of time before the Micro800 controller sends the packet.The value is from 0 through 65535. The default value is 0. |
RTS off delay | Specifies the delayed amount of time between the end of a transmission and the Ready To Send (RTS) drop. It is available when Half Duplex without continuous carrier (RTS/CTS) is selected for Control line .The value is from 0 through 32767. The default value is 0. |
RTS send delay | Specifies the delayed amount of time between the activation of RTS and the initiation of a transmission. It is available when Half Duplex without continuous carrier (RTS/CTS) is selected for Control line .The value is from 0 through 32767. The default value is 0. |
Polling ranges | Specifies a continuous range of intervals at which the slave polls for data. It is available when Polling mode is set to Standard .You can set a priority polling range and a normal polling range by supplying station addresses for the devices to poll. Slaves in the priority polling range are polled more frequently than slaves in the normal polling range. Normal poll group size specifies active stations that are polled from the normal poll node list.The value is from 0 through 255. |
Provide Feedback