DF1 half-duplex slave configuration page
Use information in the following table to configure a DF1 half-duplex slave.
Setting | Description |
|---|---|
Media | Specifies the supported media type. The available options are RS232 and RS485 . RS232 is the default option. |
Control line | Specifies the type of handshake that is used for communication.
|
Error detection | Specifies the error detection scheme for message transmission.
CRC is the default option. |
EOT suppression | Determines whether to turn on response suspension using an EOT when the master polls the slave. Turning on EOT suppression reduces the number of modem transmissions from the slave, which is important in solar power applications but will lead the master to consider the slave as not active. |
Duplicate packet detection | Determines how duplicate messages are handled.
Duplicate packet detection is selected by default. |
Poll timeout | Specifies the amount of time that the slave will anticipate a poll from the master following the activation of an MSG instruction. It is applied when the slave initiates an MSG instruction. The value is from 0 through 32767, with each unit increment representing 20 milliseconds. The default value is 3000 . |
Message retries | Specifies the count of retry attempts by an slave to resend a message packet in the absence of an acknowledgment (ACK) from the master. The parameter can be used in noisy environments, where message packets might be corrupted during transmission. The value is from 0 through 127. The default value is 3. |
Pre-transmission delay | Specifies the amount of time before the Micro800 controller sends the packet.The value is from 0 through 65535. The default value is 0. |
RTS off delay | Specifies the delayed amount of time between the end of a transmission and the Ready To Send (RTS) drop. It is available when Half Duplex without continuous carrier (RTS/CTS) is selected for Control line .The value is from 0 through 32767. The default value is 0. |
RTS send delay | Specifies the delayed amount of time between the activation of RTS and the initiation of a transmission. It is available when Half Duplex without continuous carrier (RTS/CTS) is selected for Control line .The value is from 0 through 32767. The default value is 0. |
Provide Feedback