DF1 radio modem configuration page
Use information in the following table to configure a DF1 radio modem.
Setting | Description |
|---|---|
Media | Specifies the supported media type: RS232 . |
Control line | Specifies the type of handshake that is used for communication.
|
Error detection | Specifies the error detection scheme for message transmission.
CRC is the default option. |
Pre-transmission delay | Specifies the amount of time before the Micro800 controller sends the packet.The value is from 0 through 65535. The default value is 0. |
RTS off delay | Specifies the delayed amount of time between the end of a transmission and the Ready To Send (RTS) drop. It is available when Half Duplex without continuous carrier (RTS/CTS) is selected for Control line .The value is from 0 through 32767. The default value is 0. |
RTS send delay | Specifies the delayed amount of time between the activation of RTS and the initiation of a transmission. It is available when Half Duplex without continuous carrier (RTS/CTS) is selected for Control line .The value is from 0 through 32767. The default value is 0. |
DCD wait delay | Specifies the time to wait for the DCD to become low before returning errors. The option is available when Half-duplex with DCD handshake is set for Control line . The value is from 0 through 8191. The default value is 0. |
Enable Store and Forward | Turns on or turns off the Store and Forward function when receiving a message. |
Store and Forward type | Specifies the store and forward type.
The supported data types of variables:
|
Provide Feedback