DF1 full-duplex configuration page
Use information in the following table to configure a DF1 full-duplex.
Setting | Description |
|---|---|
Media | Specifies the supported media type. The available option is RS232 . |
Control line | Specifies the type of handshake that is used for communication.
|
Error detection | Specifies the error detection scheme for message transmission.
CRC is the default option. |
Embedded responses | Specifies how the controller sends embedded messages. If the controller is transmitting a message and concurrently receives a complete message, it can positively acknowledge (ACK) or negatively acknowledge (NAK) the newly received message within the ongoing transmission. There is no need to send a message only for conveying an ACK or NAK. Options are as follows:
|
Duplicate packet detection | Determines how duplicate messages are handled.
Duplicate packet detection is selected by default. |
ACK timeout | Specifies the duration that the controller waits for an acknowledgment after transmitting a message. The value is from 0 through 32767, with each unit increment representing 20 milliseconds. The default value is 50 (50 * 20 milliseconds, 1,000 milliseconds, or 1 second). |
NAK retries | Specifies the number of NAKs that the controller can receive in response to a message before stopping the transmission. The value is from 0 through 127. The default value is 3. |
ENQ retries | Specifies the number of inquiries that the controller sends to the target after an internal ACK timeout. If the controller does not receive an ACK from the target, another inquiry is sent (send ENQ), requesting an acknowledgment before a full retransmit of the original message. The value is from 0 through 127. The default value is 3. |
Provide Feedback