Open the FBAxis<x> configuration pages

In
FactoryTalk Design Workbench
, a 2080-MOT-HSC plug-in module that is added to the controller project can be enabled with
Feedback Axis
.
After adding a 2080-MOT-HSC plug-in module and activating it with
Feedback Axis
:
  • On the
    2080-MOT-HSC
    configuration page, a
    Feedback Axis
    node is created. Select the node to view and configure the settings on the following pages:
  • On the PTO Motion configuration page, a
    FBAxis<x>
    checkbox is added. The checkbox is selected and read-only by default.
To open the FBAxis configuration page
  1. In
    Project Organizer
    , go to
    I/O Configurations
    Plug-in
    , and then double-click
    2080-MOT-HSC
    .
  2. On the
    2080-MOT-HSC
    page, select
    Feedback Axis
    .
  3. Select General, Motor and load, or Limits to view or change the corresponding settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal