FBAxis - Motor and Load tab
Use the
FBAxis<x> - Motor and Load
configuration page to do the following actions:- Select the unit scaling that matches your mechanical system values.
- Specify the number of pulses for one revolution of the motor.
- Specify the distance covered by the load in one revolution of the motor.
Category | Description | |
|---|---|---|
User-defined Unit | Specifies the unit scaling that matches your mechanical system values. The units are applied across all commands and axis user unit values for programming, configuration, and monitoring functions.
| |
Motor Revolution | Pulses per revolution | Specifies the number of pulses for one revolution of the motor. The value is from 0.0001 through 8388607 in single precision floating format. The default value is 200.0. |
Travel per revolution | Specifies the linear or rotational distance covered by the load in a revolution of the motor. The value is from 0.0001 through 8388607 in single precision floating format, measured in the User-defined Unit . For example, 1.0 mm. | |
Provide Feedback