FBAxis - General tab
Use the
FBAxis<x> - General
configuration page to do the following actions:- Rename the FBAxis.
- Pair the FBAxis with a pulse train output (PTO) axis when a PTO axis is part of the controller configuration.
- Specify the motion encoder type when the FBAxis is paired with an encoder.
Setting | Description |
|---|---|
Axis name | Specifies the name of the feedback axis. The axis name must be unique and cannot be the same with an existing variable name, data type, or reserved word. The naming conventions of an axis name are as follows:
|
Pairing with | Specifies with which axis the FBAxis is paired. Options are as follows:
When a motion feedback axis is set, it is read-only and cannot be changed until you cancel the pairing. When a PTO axis that is paired with the FBAxis is deleted, the Pairing with selection changed to the default setting Encoder . |
Encoder type | Specifies the motion encoder type that is used to send feedback information for the FBAxis.
Options are as follows:
Quadrature X4 is the default type. The options are available when you set Pairing with to Encoder . |
Provide Feedback