Work Unit Level Dashboard

Offers granular insights into energy usage at the work-unit level. It enables precise tracking of energy consumption for individual machines or processes, facilitating targeted energy-saving actions and maintenance planning.
Click
Work Unit
from the hierarchy list.
The following table provides the list of charts available by default in the dashboard:
Chart Types
S.No
Chart/Widget Name
Description
1
Resources (Donut Charts)
Energy
: This is the overall summary of the total energy consumption, with the values of each resource type along with default units.
Cost
: This is the overall summary of the total cost with the values of each resource type.
Emission
: This is the overall summary of the resource emission, with the values of each resource type.
The table displays the top 3 resource types.
A list of resource types is displayed on clicking the expand icon on the top left corner of the widget.
In the expanded view, all the records are listed.
2
Energy Consumption by Resource Type
The user can view the selected time period with the respective granularity on the X-axis and consumption on the Y-axis. This chart shows the overall energy consumption summary with default values (hover the mouse and you see the data with default values).
3
Costs by Resource Type
The user can view the selected time period with the respective granularity on the X-axis and cost on the Y-axis. This chart shows the overall energy cost summary.
4
Emissions by Resource Type
The user can view the selected time period with the respective granularity on the X-axis and emissions on the Y-axis. This chart shows the overall emission summary.
5
Energy Intensity
The user can view the selected time period with the respective granularity on the X-axis and energy intensity on the primary Y-axis, production data on the secondary Y-axis. This chart shows the overall energy intensity summary with the comparison of production data.
6
Production Data
The user can view the selected time period with the respective granularity on the X-axis and production data on the Y-axis. This chart shows the overall production summary.
7
Total Consumption - Production Chart
The user can view the selected time period with the respective granularity on the X-axis and consumption in the primary Y-axis, and production data in the secondary Y-axis. This chart shows the overall consumption summary with the comparison of production data.
8
Resource / Utility Consumption Data
The user can view the consumption of the configured resource/utility of the selected time scope with the respective granularity on the X-axis and consumption details on the Y-axis.
9
Resource / Utility Demand Data
The user can view the demand of the configured resource/utility of the selected time scope with the respective granularity on the X-axis and demand details on the Y-axis.
10
Energy Consumption (Heat Map)
The X-axis and Y-axis granularity values are represented based on your time period selection. This chart shows the overall consumption summary in the heat map format with color representation.
Refer to Dashboard Features section to manage the Work Unit-Level dashboard.
Related Information
:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal