Highlight Settings dialog box

How do I open the Highlight Settings dialog box?
In the Object Explorer, select
Highlighting on
and click
Settings
.
Use the
Highlight Settings
dialog box to highlight specified objects on the graphic display and the
Object Explorer
tree list.
You can select objects by object type, animation type, or tag name.
Objects with the selected properties are highlighted in red on the graphic display and in the
Object Explorer
. If your graphic display uses a red background, you will not be able to see the highlights.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal