Object Explorer
How do I open the Object Explorer?
When you open a project, the
Object Explorer
is shown on the right in the main window. You can hide it, and change its size and position. If it is not shown, open it using one of the following methods:- On theGraphicstoolbar, click
. - From theViewmenu, selectObject Explorer.
- Right-click an object and selectObject Explorer.
Object Explorer
provides a tree-list naming all the objects on the graphic display and allows you to select, hide, and highlight objects from the list. Groups are listed as expandable items in the tree, with a + icon.You can use the
Object Explorer
to:- Select an object that is hidden behind other objects on the graphic display, without bringing the object to the front. Objects are listed in front-to-back order. The object you created most recently is at the front, unless you move it back using theSend to Backoption.
- Show or hide an object on the graphic display by selecting or clearing the checkbox in front of the object in theObject Explorer.
- Highlight objects by object type, highlight objects that have animation attached, and to highlight objects with specific tag or expression assignments.
The
Object Explorer
does not show wallpaper objects or objects within ActiveX composite objects.
TIP:
- When you right-click the root node,Displayin theObject Explorer, a context menu shows. The menu is the same menu that you would see if you right-click on the graphic display.
- When you right-click a graphic object or group in theObject Explorer, the context menu for that object or group shows. The menu is the same menu that you would see if you right-click the object or group on the graphic display, except that theObject Explorermenu item does not show.
- When you double-click most graphic objects in theObject Explorer, including drawing objects, the object'sPropertiesdialog box opens. For ActiveX objects, the behavior of the object when double-clicked depends on the vendor's implementation.
Provide Feedback