Options in the Object Explore
The following table shows the options in the
Object Explorer
.Options | Descriptions |
|---|---|
Highlight on | Select this check box to highlight the objects specified in the Highlight Settings dialog box on the graphic display and the Object Explorer tree list. You can select objects by object type, animation type, or tag name. |
Settings | Click Settings to open the Highlight Settings dialog box. |
Expand | Use the Expand button to expand all the groups in the list at once. |
Collapse | Use the Collapse buttons to collapse all the groups in the list at once. |
Provide Feedback