Highlight Settings
    How do I open the Highlight Settings dialog box?
        
In the Object Explorer, select 
Highlighting on
 and click Settings
.Use the 
Highlight Settings
 dialog box to highlight specified objects on the graphic display and the Object Explorer
 tree list.You can select objects by object type, animation type, or tag name.
Objects with the selected properties are highlighted in red on the graphic display and in the 
Object Explorer
. If your graphic display uses a red background, you will not be able to see the highlights.Provide Feedback