Options in the Highlight Settings dialog box
    The following table shows the options in the 
Highlight Settings
 dialog box.Options  | Descriptions  | 
|---|---|
By object type  | Select one or more object types in the list.  | 
By animation type  | Select one or more animation types in the list.  | 
By tag name  | Select  By tag name , and then select a tag name or expression from the list. The list shows all the tags and expressions referenced by objects on the graphic display (except the tags contained in embedded variables). | 
Provide Feedback