- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Create project variables
Create the Speed and Acceleration variables to use them in the UI design.
- InProject view, create two variables by right-clicking theModelfolder, and selecting .
- Rename the variables by hovering-over each variable, selecting, and entering:
- Speed
- Acceleration
Provide Feedback