The area module and command verification policies
The area model supports several types of command verification policies that can generate signature requests before, during, or when batch execution is complete.
Actions initiated in or through the .
FactoryTalk Batch View
, FactoryTalk Batch View HMI Controls
, e
ProcedureFactoryTalk Batch
Server API, generate signature requests. For
information on executes, see the FactoryTalk Batch
Server API Communication Language Reference
GuideProvide Feedback