FactoryTalk Batch electronic signatures

FactoryTalk Batch
electronic signatures are electronically recorded representations of a signature and their associated data. Signature data includes time stamps, security permissions, meanings for signoffs, and comments. When a signature request is created, an entry is recorded in the Event Journal. If the signature request is user generated, a
Signature
dialog box is displayed. Additional journal entries are recorded when a signature request is completed, user canceled, system canceled, or when a signoff is successful or unsuccessful. These electronic signatures include all the components necessary for compliance with 21 CFR Part 11.
A
Signature
dialog box displays context information to the user based on the signature request type. For example, a
Command Signature
dialog box displays
Time Generated
,
Batch ID
,
Procedure ID
, and
Command
.
There are several steps involved in configuring and executing electronic signatures.
IMPORTANT:
The
FactoryTalk Batch
Server responds differently when electronic signatures are configured in the area model. Be aware of the behavior changes before a decision is made to implement electronic signatures.
The requested user information in a
Signature
dialog box is defined by the signature template configured in the area model. Signature templates determine the number of signoffs required to complete a signature request. Each signoff has associated security permissions, meaning, and may require a comment. Signature templates are used with:
  • Command Verification Policies
  • Parameter Deviation Verification Policies
  • General Usage Phase Logic Requests
  • e
    Procedure
    Step Verifications
Signature templates are used to generate signature requests displayed in
FactoryTalk Batch View
,
FactoryTalk Batch View HMI Controls
, and
e
Procedure
.
Signature templates determine the credentials and number of signoffs required for steps defined as part of a Recipe Approval process.
See the for information on configuring signature templates.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal