Add Event Signature request
Overview
If a Comment Command Verification policy is configured in the area model and it is
associated with a Signature Template, then an .
Add Event
Signature
Request is generated when a user attempts adding a comment
to a batch. For information on the AddEvent execute, see the FactoryTalk Batch
Server API Reference Manual
, publication BATCH-RM003
Modifications for FactoryTalk Batch electronic signatures
AddEvent Execute | |
|---|---|
Batch Server | When the FactoryTalk® Batch Server receives a legal
AddEvent, AddEvent_Phase, or AddEvent_CI execute, it checks the
Area Model configuration to decide if a confirmation Signature
is required for the AddEvent action. If one is required, then a
Signature Request is generated using the specified Signature
Template and the AddEvent action is queued pending completion of
the Signature Request.An AddEvent is not generated when all batches are selected. |
Response | An ActionID is returned by the execute used to locate the
generated signature. |
Completion | When all Signature Signoffs associated with an AddEvent execute
are completed, then the AddEvent action is handled if it is
still legal. |
Cancellation | When any Signature generated by an AddEvent execute action is
cancelled, then the AddEvent execute action is terminated and
its associated incomplete Signature Requests are System
Cancelled. |
Overlap | AddEvent executes targeted at the same batch are permitted to
overlap. If the batch has a Remove Action pending, then AddEvent
execute fails. |
Warm Restart, Warm All Restart, or Hot Restart | Signature Requests generated in response to a AddEvent execute
action are cancelled in the event of a FactoryTalk Batch Server Warm Restart, Warm All Restart, or Hot Restart. |
Provide Feedback