Search
PointMax Digital I/O Modules Add-on Profile Online Help
Ptxx view (Universal Digital Modules)
Use
Ptxx
to view or configure a specific point of the device.
Points view (Universal Digital Modules)
XX – Input view parameters (5034-UB8, 5034-UB8F)
XX – Input, Timestamp view parameters (5034-UB8, 5034-UB8F)
XX – Input, Counter view parameters (5034-UB8, 5034-UB8F)
XX – Input, FIFO view parameters (5034-UB8F)
XX – Output (Scheduled) view parameters (5034-UB8)
XX – Output (Scheduled) view parameters (5034-UB8F)
XX – Output (Scheduled), PWM view parameters (5034-UB8F)
XX – Output, Logic Controlled view parameters (5034-UB8F)
XX – Output, Triggered Pulse view parameters (5034-UB8F)
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal