XX – Output, Triggered Pulse view parameters (5034-UB8F)
The
XX – Output, Triggered Pulse
view includes these parameters:
Parameter | Description |
|---|---|
Triggered by | Specifies the input that triggers the pulse function.
|
Invert Trigger | This option inverts the trigger edge for the input point
selected in the 'Trigger by' parameter.
|
Pulse Delay | Specifies the delay time in seconds between the trigger event
and the start of the output pulse. |
Pulse Active Time | Specifies the active duration in seconds for the generated
output pulse. |
Output State in Program Mode Program State | Determines the behavior of each output when the controller
transitions to Program Mode or Inhibit mode. While in
Program Mode or Inhibit mode, outputs from the controller
are ignored and the output behaves as follows:
|
Output State in Communication Fault Mode Communication Fault State | Determines what happens to the output of each point after a
communication fault occurs and the module enters
Communication Fault Mode.
|
Output State in Communication Fault Mode Communication Fault State Duration | Determines the length of time the Communication Fault Mode is
held before the Final Fault State. |
Output State in Communication Fault Mode Final Communication Fault State | Determines whether the module transitions to On or Off after
the Communication Fault Mode Output State Duration elapses.
The default final state is Off. If you choose Forever for Duration, you cannot choose a final
state. The module retains its current Communication Fault
Mode state. |
Output State When Communication Fails in Program Mode | Determines the output action if communication fails in
Program Mode.
|
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback