XX – Input view parameters (5034-UB8, 5034-UB8F)

The
XX – Input
view includes these parameters:
Parameter
Description
Power Source
Defines the power source for the point.
  • Ptxx – Power is supplied to the sensor from point xx of this module, which is configured to function as a power supply.
    If a short circuit is detected on the Power Supply point, the fault is rolled-up to the Digital Input point.
  • External – Power is supplied to the sensor from an external power supply.
  • SSV – Power is supplied to the sensor from the SSV terminal of this module.
    If an SSV short circuit is detected, the fault is rolled-up to the Digital Input point.
Input Filters
Off → On Filter Time
Defines how long an Off to On input transition must remain in the On state before the device considers the transition valid.
Input Filters
On → Off Filter Time
Defines how long an On to Off input transition must remain in the Off state before the device considers the transition valid.
Diagnostics
Opens the Diagnostics dialog, which contains diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal